Buscar obras de referencia

Mostrar 51 a 60 de 106 resultados
Case banner
Grundfos pumps in 1,000 m3/day RO plant in Algeria
Astramatic S.A., Barcelona, Spain, is an engineering and consulting company that designs, builds, manufactures, and maintains industrial process water treatment plants adapted to all needs and situations.
Grundfos sanitary pumps handle media with high viscosity
Nordzucker, based in Nordstemmen Germany, is a leading producer of sugar and a supplier of natural sweeteners. Their core business includes extraction and processing of sugar for the food industry as well as a wide variety of sugar products for the retail industries and for household use.
Grundfos sanitary range at Jacobsen’s Brewhouse
The kettles at The Jacobsen’s Brewhouse on the Carlsberg property in Copenhagen are brewing specialty beer as ever before. Over the past couple of years, the beer market has taken a U-turn and consumers increasingly demand beer of a quality that reflects old taste and tradition.
Grundfos solves problems with corrosion in cavern plant
The ARA Tobl is nothing short of a technological wonder. It is the first wastewater treatment plant to be built in a cavern and the only one of its kind in central Europe.
Grundfos suministra un bombeo fiable y de bajo coste en Guadalajara, México
La perla de México del oeste, Guadalajara es la segunda ciudad más grande del país. Al visitar la ciudad, se sumergirá en una metrópolis muy ocupada, albergando uno de los mayores centros culturales y de negocios.
Grundfos thinks outside of the box in Costa Rica
The capital of Costa Rica, San José is fascinating. It was founded in 1737, but didn’t really experience great importance to Costa Rican society until the end of the nineteenth century. Even so, its population was small as late as the 1950’s, until growing to over 1,000,000 today.
Grundfos wastewater pumps suitable for clean water, too
EL OBOUR CITY, EGYPT: The community of El Obour City is one of the 16 “New Towns” designed to alleviate housing shortages in the main cities of Cairo and Alexandria. Located approximately 35 km away from Cairo, El Obour City is intended to house a total of 250,000 inhabitants. Large-scale Grundfos pumps originally designed for wastewater applications were chosen to provide the community with water for domestic use.
Hast Akku: How heating and hot water cost less
MSR-Service GmbH (Managing Directors: Dipl.-Ing. Bruno Schramm and Dipl.-Ing. Gabriela Schramm) was founded in 1992 and employs 14 members of staff. Since the company was founded, the team of engineers, technicians, master craftsmen and skilled workers has been working on the implementation of cost saving and energy saving heating, air conditioning and sanitation systems. The HAST-AKKU concept was developed from this – the system makes it possible to make considerable cost and energy savings ...
High ambitions for Moscow’s Tower 2000
The prestigious Moscow City project covers 100 hectares in Moscow’s central business district, and is due to be completed in 2010. Often described as Moscow’s first “smart building”, the 34-storey Tower 2000 complex contains offices, retail stores, restaurants, underground parking and an observation platform that provides spectacular views of the city.
High pressure pump for RO plant
Weil Industrieanlagen GmbH is a specialist in water purification and water treatment and was established in 1986. The water purification and water treatment techniques both use membrane technology, (reverse osmosis, nano-filtration, and micro-filtration). The company focuses mainly on three technology areas: building technology, energy technology and pharmaceutical and medical technology.